Programming External Flash using CFv2 JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming External Flash using CFv2 JTAG

Jump to solution
1,991 Views
kunalgaur
Contributor I

Hello,

 

we are using a custom board, with Coldfire V2 processor, and external Spansion flash. earlier the board was using BDM interface, and programming spansion flash was easy using P&E micro CYCLONE MAX. however due to design change in custom board, currently we are using JTAG interface instead of BDM.

I have this query for programming external flash using JTAG interface, as P&E micro does not support programming from JTAG.

Does anyone know any tool available in market which can support programming to external flash with CFv2 JTAG support?

 

Thanks & Regards,

Kunal Gaur

Labels (1)
0 Kudos
Reply
1 Solution
1,796 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello kunal

Sorry please be note that ColdFire debugging and programming can only be done with BDM. JTAG is only for scan testing.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

View solution in original post

0 Kudos
Reply
2 Replies
1,797 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello kunal

Sorry please be note that ColdFire debugging and programming can only be done with BDM. JTAG is only for scan testing.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

0 Kudos
Reply
1,796 Views
kunalgaur
Contributor I

Thank you.

Regards,

Kunal Gaur

0 Kudos
Reply