Program running out

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program running out

2,268件の閲覧回数
gm2010ustc
Contributor I

XEP100 MCU,When the program runs into the update function,run to PFlash_EraseSectorBySector(0x7C0000UL, 0x7FDFDFUL);

when  this program is run over,it  jump directly to the ZeroMem function,then the Program running out.  I don't know why this happen.

Original Attachment has been moved to: bootloader_debug_20151030.rar

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,090件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

this thread was posted two years ago.

Please create a new thread for your specific question.

I would suggest you attach the error screenshot and demo project of the problem.

Jennie Zhang

0 件の賞賛
返信

2,090件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi,

I have answered you in SR1-4142120521,

please refer the demo code to make your own project.

thanks!


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,090件の閲覧回数
tafengchung
Contributor II

I have the same question,

why? and how to fixed this issue?

0 件の賞賛
返信