Program flash via CAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program flash via CAN

3,890件の閲覧回数
AndersJ
Contributor IV
I need to field-update a HCS12 application via CAN.
Basically CAN-based "serial bootloader".
 
Any pointers, or good ideas, anyone?
 
Thanks,
Anders Johansson
 
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,489件の閲覧回数
suchita
Contributor I

I have your application note for Flash programming via CAN (AN1828), I have gone through that , In this I want to know that you are saying that in bootloader code it checks for value of $C000, $C001 address register if it is cleare then it will go for flash programming via CAN , But i not getting i will clear this register, So if any oen of you can tell then pls tell me when i will clear this register

0 件の賞賛
返信

1,489件の閲覧回数
bigmac
Specialist III

Hello Anders,

Have a look at AN1828 - although it may be a little old.

Regards,
Mac