Program/Flash script for MC9S08JM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program/Flash script for MC9S08JM

ソリューションへジャンプ
1,644件の閲覧回数
leesp
Contributor I

I am currently using "True-time Simulator & Real-time Debugger" and PEMicro's USB Multilink to program my MC9S08JM. The problem is that the user interface has a few buttons to be clicked.. and this is troublesome.

Is there a way which I can use some scripts to automate the flashing? i.e just enter a command at the command-line and the rest is automated?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,455件の閲覧回数
bigmac
Specialist III

Hello,

 

P&E sell a command line programmer for MC9S08 devices.  The program cproghcs08 is part of their HCS08 software package.

 

The True-time Simulator and Real-time Debbugger program can be run stand-alone, without use of the CW IDE, but I am not sure whether this will solve your problem.

 

Regards,

Mac

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,456件の閲覧回数
bigmac
Specialist III

Hello,

 

P&E sell a command line programmer for MC9S08 devices.  The program cproghcs08 is part of their HCS08 software package.

 

The True-time Simulator and Real-time Debbugger program can be run stand-alone, without use of the CW IDE, but I am not sure whether this will solve your problem.

 

Regards,

Mac

 

0 件の賞賛
返信