Program/Flash script for MC9S08JM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Program/Flash script for MC9S08JM

跳至解决方案
1,653 次查看
leesp
Contributor I

I am currently using "True-time Simulator & Real-time Debugger" and PEMicro's USB Multilink to program my MC9S08JM. The problem is that the user interface has a few buttons to be clicked.. and this is troublesome.

Is there a way which I can use some scripts to automate the flashing? i.e just enter a command at the command-line and the rest is automated?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,464 次查看
bigmac
Specialist III

Hello,

 

P&E sell a command line programmer for MC9S08 devices.  The program cproghcs08 is part of their HCS08 software package.

 

The True-time Simulator and Real-time Debbugger program can be run stand-alone, without use of the CW IDE, but I am not sure whether this will solve your problem.

 

Regards,

Mac

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,465 次查看
bigmac
Specialist III

Hello,

 

P&E sell a command line programmer for MC9S08 devices.  The program cproghcs08 is part of their HCS08 software package.

 

The True-time Simulator and Real-time Debbugger program can be run stand-alone, without use of the CW IDE, but I am not sure whether this will solve your problem.

 

Regards,

Mac

 

0 项奖励
回复