Processor expert with xgate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor expert with xgate

ソリューションへジャンプ
2,375件の閲覧回数
itisravi
Contributor II

Hi,

 

Has anyone successfully used PE beans with Xgate? Apparenty  PE (2.98) does not have support for Xgate yet. I've used PE to generate SCI (uart) code for hadling interrupts/events. I need the interrupt (and all events/ functions assoicated with it) to be redirected to xgate.

 

The normal way (without using beans) would be:

1. Direct the interrupt event to the XGATE. (RQST bit)
2. Create a thread to handle the interrupt.(i.e. an interrupt handler)
3. Initialize the XGATE interrupt vector table to point to the thread.

 

What do i need to modify in the PE genereated code to achieve the same?

 

Thanks.

Ravi

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,549件の閲覧回数
ProcessorExpert
Senior Contributor III
Hello,
 
Processor Expert does not support the XGATE at this time. However https://community.freescale.com/message/56367#56367 link should help you to add XGATE feature into Processor Expert project.
best regards
Vojtech Filip
Processor Expert Support Team

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,550件の閲覧回数
ProcessorExpert
Senior Contributor III
Hello,
 
Processor Expert does not support the XGATE at this time. However https://community.freescale.com/message/56367#56367 link should help you to add XGATE feature into Processor Expert project.
best regards
Vojtech Filip
Processor Expert Support Team
0 件の賞賛
返信