Processor Expert w/ CW 4.6 for HCS12 problems locking up?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert w/ CW 4.6 for HCS12 problems locking up?

3,595 Views
baddad
Contributor I
I am using CW 4.6 for the HCS12.
 
When I try to launch Processor expert, I get windows execution error messages and PE locks up while starting.  CW continues to work, but the PE window is locked in front of everything else.
 
Has anyone else seen this problem?
Any idea whats going on?
 
I've re-installed it twice, but still the same thing.
 
I also have CW 5.1 and 6.0 installed and they both work fine.
 
BadDad


Message Edited by baddad on 2007-07-27 06:55 PM
Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,079 Views
Phoenix
Contributor III
Hello BadDad
 
Oh, strange. What version of windows do you use?
 
>I also have CW 5.1 and 6.0 installed and they both work fine.
 
Do you mean processor expert works fine in this versions?
 
>When I try to launch Processor expert, I get windows execution error messages and PE locks up while starting.  CW continues to work, but the PE window is locked in front of everything else.
 
What execution error? Is this behaviour the same with any MCU or did you try it just with one of them?
Did the Processor expert with CW4.6 works on your machine well before or is it new installation?
 
Regards
 
Phoenix

2,079 Views
Phoenix
Contributor III
So I finished tests:
I installed clean WindowsXP (you did not mention OS version), then CW5.1, CW6.0 and CW4.6.. first project with PE tooks little more time to create (hang for approx 45s on PE init), but then everything works fine.
 
Please provide more information.
Meanwhile I can suggest you clean-up procedure (see attachement) - but it is a little bit time consuming.

2,079 Views
baddad
Contributor I
I am running Windoze XP (tablet PC version).
 
The first error is "access violation at address 0013CFB1.  Write of address 00000001."
 
Then "access violation .... in module "PE_Plugin.dll"..."
 
Then PE just sits on it's opening screen and never gets any further.
 
PE works fine in each of my HC08 versions of CW.
 
BadDad
0 Kudos
Reply