Processor Expert performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert performance

Jump to solution
3,148 Views
SSK
Contributor I
Dear Forum Members,
 
I am using MC9S12GC32CPB16 in one of my projects. I am using Codewarrior 4.6 build 6345. I am using Processor Expert feature for my project coding. While working on the code, I came across a discussion on optimization  for code size and execution speed. Whether code generated by Processor expert adds extra overhead from size as well as execution point of view for overall project code? Whether it is beneficial to use Processor expert though it eases coding for processor peripherals? I am using SPI, SCI, Simulated SPI, Watchdog, Timer, Capture, RTI, BitIO beans for my project. Your earliest help in this regard will help me decide whether to use PE or standard way of coding.
 
Thanks in advance.
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,970 Views
ProcessorExpert
Senior Contributor III
Processor Expert generates peripheral drivers code depending on the bean settings.

Information about possible optimalization of the generated code can be found in the chapter Embedded Beans Optimizations (Application Design/Embedded Beans Optimizations) in the help of  Processor Expert (menu command Help/Processor Expert/Processor Expert Help).

Please don´t miss also  information about optimalization through the Configuration inspector in the chapter Configuration Inspector (User Interfece/Inspector) in the menu command Processor Expert Help.

View solution in original post

0 Kudos
Reply
2 Replies
1,971 Views
ProcessorExpert
Senior Contributor III
Processor Expert generates peripheral drivers code depending on the bean settings.

Information about possible optimalization of the generated code can be found in the chapter Embedded Beans Optimizations (Application Design/Embedded Beans Optimizations) in the help of  Processor Expert (menu command Help/Processor Expert/Processor Expert Help).

Please don´t miss also  information about optimalization through the Configuration inspector in the chapter Configuration Inspector (User Interfece/Inspector) in the menu command Processor Expert Help.

0 Kudos
Reply
1,969 Views
J2MEJediMaster
Specialist I
This isn't relevant to this discussion, but needs to be said:

Please do NOT post the same question to different forums! It causes confusion and has people spend their valuable time (particularly the contributors) answering the same subject. I have deleted the posting in the CodeWarrior General forum.

---Tom


0 Kudos
Reply