Processor Expert for MPC5676R

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert for MPC5676R

1,821 Views
thomasolenik
Contributor III

I've been using Processor Expert for a while with various Kinetis series processors. I'm just beginning to evaluate the MPC5676R in CodeWarrior for MCU and do not see any Processor Expert support. Processor Expert seems to be installed and components are available for Kinetis, but not MPC5676R.  Are processor components available for installation for this MCU? If not, are there other similar tool alternatives for the MPC5676R?

 

Thanks,

 

Tom

Labels (1)
0 Kudos
Reply
1 Reply

1,690 Views
TICS_Fiona
NXP Employee
NXP Employee

Processor Expert does not support MPC56xx family, we use another tool called RAppID:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RAPPID

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply