Processor Expert for MPC5676R

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert for MPC5676R

1,852件の閲覧回数
thomasolenik
Contributor III

I've been using Processor Expert for a while with various Kinetis series processors. I'm just beginning to evaluate the MPC5676R in CodeWarrior for MCU and do not see any Processor Expert support. Processor Expert seems to be installed and components are available for Kinetis, but not MPC5676R.  Are processor components available for installation for this MCU? If not, are there other similar tool alternatives for the MPC5676R?

 

Thanks,

 

Tom

ラベル(1)
0 件の賞賛
返信
1 返信

1,721件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Processor Expert does not support MPC56xx family, we use another tool called RAppID:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RAPPID

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信