Processor Expert Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert Error

1,686件の閲覧回数
cd
Contributor I

Hello,

 

I use the processor expert version 10.4.0 and try to work with a project generated by another person (using version 10.3.0). I get the following error:

 

DescriptionResourcePathLocationType
ERROR: Unexpected status of script: Beans\ADC\ADC_LDD.chg, please contact Freescale support.peripheryVAA_POS_ADCProcessor Expert Problem

 

So here I am.

 

Thank you for help in advance,

 

Christian

ラベル(1)
0 件の賞賛
返信
1 返信

1,307件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Christian:

This was a Processor Expert bug (check this).

The bug was fixed with PEx 10.4 Update 1 (10.4.1), but there is now an Update 2 (10.4.2), so I recommend you to install the latest so you have PEx 10.4.2.

For more details and installation instructions please check the next document in the community:

Processor Expert Driver Suite Update 10.4.2 available!


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信