Problem with write program pernamently to target

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with write program pernamently to target

2,171件の閲覧回数
lucast
Contributor I

Hello,

I just start working with CodeWarrior 10.6 (before CodeWarrior IDE) and I have a problem with runing downloaded programm. When I click debug button and after download F8 - my program is working correctly but when I just swith off and then swith on power - program can't start.

 

In codewarrior IDE was be ok.

My program is very simple(LED flashing) and configuration is default.

 

Could anybody know what is wrong?

 

 

regards

Lukasz

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,043件の閲覧回数
lucast
Contributor I

Thank You for answer.

I found what was a reason.

After changing parameter in PE configuration: CPU->Internal peripherals->Bootloader->Flash Block 1->Checksum  from "Calculate" to "Bypass, jump to user code" it is ok.

0 件の賞賛
返信

2,043件の閲覧回数
derek_lau
Contributor III

Please make sure you are using the FLASH project but not RAM project.

0 件の賞賛
返信

2,043件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Please first make sure that you are programming the application into Flash memory.  If you have already checked that the code is programmed to Flash memory and that the watchdog is not resetting the board, please check  whether the chip is configured to boot by external signal.

If this does not help, please reply with the  part number of your target MCU.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信