Problem with using watchpoints on HCS12X with PE Multilink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with using watchpoints on HCS12X with PE Multilink

1,021件の閲覧回数
btwitche
Contributor I

I'm using CodeWarrior  to debug a Freescale MC9S12EP768 microcontroller via a PE USB  Multilink (BDM) . I have been trying to get Watchpoints to work properly for some time. In some cases the watchpoints I set will work; however,  in most cases I will, upon breaking in manually, see that the memory changed without the watchpoint ever triggering on a read or write. The watchpoint I am setting is on a one byte value in un-paged RAM. Any advice would be appreciated as this has been holding progress back for some time now.

ラベル(1)
タグ(4)
0 件の賞賛
返信
0 返答(返信)