Problem with Codewarrior for MPC5606E

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with Codewarrior for MPC5606E

1,471 Views
helenshao
Contributor II

Dear,

I'm now working with MPC5606E for Ethernet commnuication. But I can't find the chip type in the Codewarrior 10.6 when I'm setting up a new project for MPC5606E.

So which Codewarrior should I install? Thank you!

 

118585_118585.pngpastedImage_0.png

Labels (1)
0 Kudos
Reply
2 Replies

1,274 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Choose MPC5604E device. In an simplified way MPC5606E = MPC5604E + BCM89810 physical interface.

0 Kudos
Reply

1,274 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Helen

The MPC5606E microcontroller integrates MPC5604E device with the Broadcom(R) BCM89810 single-port BroadR-Reach™ 100 Mbps automotive Ethernet transceiver. So you may choose MPC5604E when creating a new bareboard project for your application.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply