Problem with CW v10.3, printf and MC56F84789

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with CW v10.3, printf and MC56F84789

Jump to solution
2,046 Views
fb1
Contributor I

Hi,

 

I am using CW v10.3 SE with a MC56F84789 micro. When i use processor expert AND printf, the debugger hangs at 99% while loading the micro, however if i create a blank project without PE and utilize printf, the entire binary loads and i am able to use the debugger. Any suggestions will be greatly appreciate. Thanks!

Labels (1)
0 Kudos
Reply
1 Solution
1,919 Views
TICS_Fiona
NXP Employee
NXP Employee

Since you are using Special Edition, I would recommend updating to CW10.5, it can be downloaded from:

http://tinyurl.com/6jo5tge

If the problem still exist, please attach your project.

View solution in original post

0 Kudos
Reply
2 Replies
1,920 Views
TICS_Fiona
NXP Employee
NXP Employee

Since you are using Special Edition, I would recommend updating to CW10.5, it can be downloaded from:

http://tinyurl.com/6jo5tge

If the problem still exist, please attach your project.

0 Kudos
Reply
1,919 Views
fb1
Contributor I

v10.5 worked, thanks!

0 Kudos
Reply