Problem programming the MC13213-SRB with BDM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem programming the MC13213-SRB with BDM

ソリューションへジャンプ
2,986件の閲覧回数
hauptman
Contributor I
Hi!

I've got a MC13213-SRB board and want to connect it via BDM to CodeWarrior.
When I start hiwave.exe and set connection to HCS08 on P&E Multilink it doesn't detect any known ports ... I've connected the SRB board to my PC via the given USB cable.

Don't know what to do, I've already read the help but it doesn't help me x.x however, other function like the embedded bootloader or the triax tool work fine via USB.
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,041件の閲覧回数
J2MEJediMaster
Specialist I
OK, when you plug the board into the USB cable and then into the PC, does:

1) The PC acknowledge that a USB device was attached? (For Windows XP you get one of those little text bubbles, or it makes a "ding-dong" sound?)

2) Do any LEDs light up on the board? Typically, on most boards you'll get a yellow LED glow for board power and a green or blue LED glow for USB communications.

---Tom

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,042件の閲覧回数
J2MEJediMaster
Specialist I
OK, when you plug the board into the USB cable and then into the PC, does:

1) The PC acknowledge that a USB device was attached? (For Windows XP you get one of those little text bubbles, or it makes a "ding-dong" sound?)

2) Do any LEDs light up on the board? Typically, on most boards you'll get a yellow LED glow for board power and a green or blue LED glow for USB communications.

---Tom
0 件の賞賛
返信
2,041件の閲覧回数
hauptman
Contributor I
Hi!

Well, I think I found the problem x.x something is broken hmm I think I need to use the embedded bootloader instead (this works fine)
0 件の賞賛
返信