Problem compiling eGUI library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem compiling eGUI library

3,037件の閲覧回数
Glogov_Kolac
Contributor II

I have an problem when I include D4D eGUI library into my project. When I try to build it, this process never ends. On some % building stops and have no progress (I wait it for one hour). I use D4D libraryy source files and code examples for Official Demo (for Kinetis K60 Tower). Is there some special procedure to include D4D in custom project and to compile it with success ?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,785件の閲覧回数
infoterm
Contributor I

I have same problem when I want to integrate eGUI in my project, like it is doed in Official Example. Here is my project! Compiling never stops, it stuck at d4d_base compiling infinitevly !!!

0 件の賞賛
返信

2,785件の閲覧回数
infoterm
Contributor I

I try to integrate D4D into my project, instead of using eGUI Official Demo. Same situation, compling infinitevly. I request support from Freescale but they don't answer. I try D4D on 4 different computers and 3 different projects and it only works with official demo. !!!

0 件の賞賛
返信

2,786件の閲覧回数
J2MEJediMaster
Specialist I

See if this https://community.freescale.com/message/94424#94424 has the solution for you.

 

---Tom