Preserving EEPROM data when programming flash on 9S08DZ60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Preserving EEPROM data when programming flash on 9S08DZ60

ソリューションへジャンプ
3,420件の閲覧回数
djsimpson
Contributor III
I am using CodeWarrior V6.1 with a P&E BDM to program a 9S08DZ60, but I don't want the EEPROM erased when I update the main flash. I have ticked the "Always preserve All EEPROM data" in the Advanced Programing / Debug Options menu in the debugger, but it makes no difference.
 
Strangley, the data is not actually erased to 0xff, but any data which was not 0xff is programmed to 0x00.
 
Can someone point me to the correct way to preserve the contents of the EEPROM?
 
Thanks
 
David
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,298件の閲覧回数
J2MEJediMaster
Specialist I
Check this forum thread and see if it has the information you need.

---Tom

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,298件の閲覧回数
mayfly
Contributor III
Hi,

I haven't tried it personally *but* apparently you're supposed to be able to protect different areas of flash by noting it somehow in the prm file.  Sorry, I don't remember much more than that.

Please post again if you get it working.



2,299件の閲覧回数
J2MEJediMaster
Specialist I
Check this forum thread and see if it has the information you need.

---Tom

0 件の賞賛
返信