Premises for PE 3.06 Service Pack

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Premises for PE 3.06 Service Pack

跳至解决方案
3,946 次查看
Kopone
Contributor IV

Hi,

 

I downloaded the PE 3.06 Service Pack for CW 6.2.

 

It lists several service packs that need to be installed beforehand, which I did, but I could not find all of them for download on the freescale site. Neither a forum nor a complete site search for these service packs brought up any results. Can I just safely ignore the warnings or is their any other way to install these yet missing service packs the installer complains about:

 

CodeWarrior Development Studio for Microcontrollers V6.2 CFV1 EM256 Service Pack
CodeWarrior Development Studio for Microcontrollers V6.2 HCS08 JS16 Service Pack
CodeWarrior Development Studio for Microcontrollers V6.2 HCS08 LG32 Service Pack
CodeWarrior Development Studio for Microcontrollers V6.2 HCS08 LH64/LL64 Service Pack
CodeWarrior Development Studio for Microcontrollers V6.2 HCS08 MP16 Service Pack

 

Thanks for your advice,

 Sven

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,300 次查看
ProcessorExpert
Senior Contributor III

These servicepacks are not necessary for the Processor Expert, unless you need to use some of these MCUs.
The reason why some of the servicepacks are not available is that these devices have not been launched to the market yet but they are already supported by Processor Expert. The LG32 and JS16 should be already released and added on the website and the other ones will come in the future.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,300 次查看
CompilerGuru
NXP Employee
NXP Employee

Did do not check it, but does the CodeWarrior Updater (see in the start menu) not install all the needed ones?

 

Daniel 

0 项奖励
回复
2,300 次查看
Kopone
Contributor IV

Well the Updater regards everything as up to date. In fact it only installed one update after I did a fresh install of CW 6.2 yesterday and then, like kind of a second update, sent me to this freescale page  were I download and installed all the additional service packs and this PE 3.06 update that asks for additional service packs that I just can't seem to find anywhere. So I am a bit confused right now. Not anything urgent, CW works fine with my current setup. I just wanted to make sure to have the latest updates installed.

 

Regards,

 Sven

0 项奖励
回复
2,301 次查看
ProcessorExpert
Senior Contributor III

These servicepacks are not necessary for the Processor Expert, unless you need to use some of these MCUs.
The reason why some of the servicepacks are not available is that these devices have not been launched to the market yet but they are already supported by Processor Expert. The LG32 and JS16 should be already released and added on the website and the other ones will come in the future.

0 项奖励
回复
2,300 次查看
Kopone
Contributor IV

Why, thanks, this cures my confusion :smileywink:


Regards, Sven

0 项奖励
回复