Power Cycle Dialog

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Power Cycle Dialog

跳至解决方案
1,885 次查看
jam_petersen
Contributor I

Processor: MC9S08EL32CTL

Emulator:  PE Microlink USB Interface

 

I was debugging my device in Code Warrior.  Everything was running fine. I was stepping through an analog conversion -- I had done several channels already when a probe slipped and the processor reset. After that the debugging session locked up and I couldn't run or step. I exited the simulator and restarted the debug session, but every time I would get the Power Cycle Dialog that tells me to recycle power to the MCU and then hit okay. I did this several times, and reinserted cables etc. but it always came up with the Power Cycle dialog. over and over. I tried a new board and it does the same thing. The processor seems fine since it runs fine on a power up not in debug mode. I'm thinking something is wrong with the emulator. How can I tell?  Both blue and amber LEDs are on. The BGND line is at 0.28V when the dialog comes up, then it goes to 2.78 when I hit okay. I have 4.98V on the 5V line.

  Thanks for any help.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,738 次查看
kef
Specialist I

What voltage you see on BGND when BDM is disconnected? Maybe EL32 internal weak BGND pullup got damaged. If you don't have any pull up resistor on BGND, then try soldering something like 4.7kOhm between BGND and Vdd. You need that voltage to rise above Vih=0.65*Vdd, which is 3.25V in your case

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,738 次查看
kef
Specialist I

What voltage you see on BGND when BDM is disconnected? Maybe EL32 internal weak BGND pullup got damaged. If you don't have any pull up resistor on BGND, then try soldering something like 4.7kOhm between BGND and Vdd. You need that voltage to rise above Vih=0.65*Vdd, which is 3.25V in your case

0 项奖励
回复