Possible to use BDM through USB redirection?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Possible to use BDM through USB redirection?

1,089件の閲覧回数
jgirard1
Contributor III

Has anyone had any luck using a BDM through USB port redirection connected to Code Warrior debugger running on a remote machine?

 

I need to work at a remote site and cannot transfer my CodeWarrior license to the laptop.

 

When I am at the remote site with the laptop, I log into my desktop development machine using Remote Desktop and use Code Warrior that way. I plug my BDM into the laptop then redirect the laptop USB port back to the desktop development machine using RemoteFX (part of Remote Desktop). The BDM appears as a local device back on the development desktop.

 

CodeWarrior debugger sees the BDM except it struggles to communicate. It cannot determine a valid IO_DELAY_CNT, etc. Perhaps the latency of the USB redirection through the Ethernet is causing the issue.

 

Does anyone have any experience doing this?

ラベル(1)
0 件の賞賛
返信
0 返答(返信)