Place variable at Absolute Address within a Segment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Place variable at Absolute Address within a Segment

Jump to solution
2,546 Views
sebasira
Senior Contributor I

Hi all!

 

I'm using CW v4.6 with HCS12...

 

I have a segment definition as (I only put what matters):

 

SEGMENTS

    PAGE_EEPROM = NO_INIT  0x0400 TO 0x0FFF;

END


PLACEMENT

    EEPROM_DATA_PAGE  INTO  PAGE_EEPROM;

END


Normally, I define a 32bits EEPROM variable as:


#pragma CONST_SEG EEPROM_DATA_PAGE

  const dword EEPROM_VARS1;

#pragma CONST_SEG DEFAULT

 

But as my project grows and so does those variables, the compiler place them wherever it wants, as long as they remain inside 0x0400 - 0x0FFF.

Now I want them to be at a fixed location so they "stay on the same place" with different firmware revisions.

 

What I did was:

 

#pragma CONST_SEG EEPROM_DATA_PAGE

  const dword EEPROM_VARS1 @0x400;

#pragma CONST_SEG DEFAULT

 

Then, looking at the .map I can see that:

 

EEPROM_VARS2                              2000       4       4       4   EEPROM_DATA_PAGE

EEPROM_VARS1                              2004       4       4       3   .abs_section_2004

 

Why EEPROM_VARS1 isn't in EEPROM_DATA_PAGE? I mean, it phisically is there, but when I want to check where is each variable this doesn't help me

 

Maybe I should do the declaration other way.

 

Thanks!

 

 

 

 

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,014 Views
kef
Specialist I
  • SEGMENTS
  •     PAGE_EEPROM = NO_INIT  0x0400 TO 0x0FFF;
  • END
  • PLACEMENT
  •     EEPROM_DATA_PAGE  INTO  PAGE_EEPROM;
  • END

  • EEPROM_VARS2                              2000       4       4       4   EEPROM_DATA_PAGE
  • EEPROM_VARS1                              2004       4       4       3   .abs_section_2004

0x2000 vs 0x400 mismatch is weird.  Is it the same with CW5.x?

  • Why EEPROM_VARS1 isn't in EEPROM_DATA_PAGE? I mean, it phisically is there, but when I want to check where is each variable this doesn't help me

Do you mean you want to see @-variable in the same section? EEPROM_DATA_PAGE instead of .abs_section_xxx? I think this is not possible. @ forces linker to place object at specific address, ignoring current const/var placement. As a result small .abs_section_XXX section is generated and you see it in map file.

  • But as my project grows and so does those variables, the compiler place them wherever it wants, as long as they remain inside 0x0400 - 0x0FFF.

Do you define EEPROM variables in different files? If so, then changing Link Order will shuffle these variables a bit. Defining them in single file may help.

Even if you define them in single file, in case some variable is not used in the code, or access routine(s) is(are) not included in execution path and optimized away, data addresses will change again. But you may use ENTRIES section in PRM file. To force linking all data from eedata.c add

   eedata.c.o:*

line to ENTRIES section in PRM file. This will guarantee all vars linked and won't change their addresses until you edit eedata.c

View solution in original post

0 Kudos
Reply
2 Replies
2,015 Views
kef
Specialist I
  • SEGMENTS
  •     PAGE_EEPROM = NO_INIT  0x0400 TO 0x0FFF;
  • END
  • PLACEMENT
  •     EEPROM_DATA_PAGE  INTO  PAGE_EEPROM;
  • END

  • EEPROM_VARS2                              2000       4       4       4   EEPROM_DATA_PAGE
  • EEPROM_VARS1                              2004       4       4       3   .abs_section_2004

0x2000 vs 0x400 mismatch is weird.  Is it the same with CW5.x?

  • Why EEPROM_VARS1 isn't in EEPROM_DATA_PAGE? I mean, it phisically is there, but when I want to check where is each variable this doesn't help me

Do you mean you want to see @-variable in the same section? EEPROM_DATA_PAGE instead of .abs_section_xxx? I think this is not possible. @ forces linker to place object at specific address, ignoring current const/var placement. As a result small .abs_section_XXX section is generated and you see it in map file.

  • But as my project grows and so does those variables, the compiler place them wherever it wants, as long as they remain inside 0x0400 - 0x0FFF.

Do you define EEPROM variables in different files? If so, then changing Link Order will shuffle these variables a bit. Defining them in single file may help.

Even if you define them in single file, in case some variable is not used in the code, or access routine(s) is(are) not included in execution path and optimized away, data addresses will change again. But you may use ENTRIES section in PRM file. To force linking all data from eedata.c add

   eedata.c.o:*

line to ENTRIES section in PRM file. This will guarantee all vars linked and won't change their addresses until you edit eedata.c

0 Kudos
Reply
2,014 Views
sebasira
Senior Contributor I

Thanks Kef!

Sorry about "0x2000 vs 0x400 mismatch is weird.  Is it the same with CW5.x?" I had two projects opened (they got some variables with the same name, and I copy the .prm of one and the -map of the other... It should have been:

EEPROM_VARS2                             400       4       4       4   EEPROM_DATA_PAGE

EEPROM_VARS1                             404       4       4       3   .abs_section_2004

Do you mean you want to see @-variable in the same section? EEPROM_DATA_PAGE instead of .abs_section_xxx?

Yes, that was the main question. And as you said, I suppose it was not possible.


Do you define EEPROM variables in different files? If so, then changing Link Order will shuffle these variables a bit. Defining them in single file may help.

Yes, I have them in a lot of differente files. Also some project share those files.


But you may use ENTRIES section in PRM file. To force linking all data from eedata.c add

   eedata.c.o:*

line to ENTRIES section in PRM file. This will guarantee all vars linked and won't change their addresses until you edit eedata.c

I didn't about about this! Thanks!

I guess I will solve the problem with the @-variable. I search those and place each variable where I want it to be.

Just to clarify a bit more, I'll explain why I asked that. We have a project which can be loaded in flash via bootloader. This project stores some user data/config in EEPROM. The bootloader don't touch EEPROM so after (re)loading code, the data/config remains untocuh.

The problem is that I notice that revision_A and revision_B of the firmware, have some of the EEPROM variables at different address so when upgrade or downgrade the data can't be correctly restore.

Thanks for helping me!

SebaS

0 Kudos
Reply