Padding and alignment in CodeWarrior for MC1321x (HCS08)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Padding and alignment in CodeWarrior for MC1321x (HCS08)

跳至解决方案
3,444 次查看
drdr
Contributor I

When creating an array of a bit field structure as in the example below, is it possible to fit two 4-bit array members into a single byte?

 

typedef struct {
  unsigned int my_location : 2;

  unsigned int my_WATCHDOG : 2;

} foo;

 

foo my_array[1000] = 0;

 

Is it possible to have the above result in 500 bytes of 1000 elements, each addressed by my_array[i] or will CW pad every element such that 1000 bytes will be used by the array?

 

Thanks for the help,

 

drdr

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,318 次查看
CompilerGuru
NXP Employee
NXP Employee

No, not with a simple foo structure.

C requires that array elements have their own addresses, therefore in order to have such a array you will have to pack a single byte in C code.

 

typedef struct {
  unsigned char my_low_location : 2;

  unsigned char my_low_WATCHDOG : 2;

  unsigned char my_high_location : 2;

  unsigned char my_high_WATCHDOG : 2;

} foo;


foo my_array[500];

 

 

Alternatively, and you can also use an array of bytes and then work with macros to implement the accesses to have a direct indexed access.


Daniel

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,319 次查看
CompilerGuru
NXP Employee
NXP Employee

No, not with a simple foo structure.

C requires that array elements have their own addresses, therefore in order to have such a array you will have to pack a single byte in C code.

 

typedef struct {
  unsigned char my_low_location : 2;

  unsigned char my_low_WATCHDOG : 2;

  unsigned char my_high_location : 2;

  unsigned char my_high_WATCHDOG : 2;

} foo;


foo my_array[500];

 

 

Alternatively, and you can also use an array of bytes and then work with macros to implement the accesses to have a direct indexed access.


Daniel
0 项奖励
回复
2,318 次查看
drdr
Contributor I

Hi Daniel,

 

Thanks for the tip.

 

drdr

0 项奖励
回复