Hi,
I am a newbie using CW for MC9S08. I noticed that there is a section _PRESTART (or .init) section which is created by the Linker automatically. In the manual it says:
"The application entry point is sotred in the segment _PRESTART. This segment also has got to be associated with a READ_ONLY section".
I checked the start08.c file but I could not find a section named _PRESTART or .init
Can anyone please advise?
Solved! Go to Solution.
 
					
				
		
Hello
The Linker will rename the section where the entry point is implemented as .init.
Per default application entry point is _Startup, which is implemented in star08.c. So section .text from module start08.c will be renamed internally as .init by the linker.
CrasyCat
 
					
				
		
Hello
The Linker will rename the section where the entry point is implemented as .init.
Per default application entry point is _Startup, which is implemented in star08.c. So section .text from module start08.c will be renamed internally as .init by the linker.
CrasyCat