PLL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PLL

1,980 Views
admin
Specialist II

Hello,

can anyone please tell me in detail how the PLL is enabled ,what and how are the calculations for the clock done?

I want to write a program using interrupts to measure the frequency of an input signal where modules like PLL, ECT are to be used. What kind of interrupt would it be like? 

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,476 Views
peg
Senior Contributor IV

Hello manasa,

 

As this is a hardware related question you should be posting in the appropriate hardware forum.

Also which device are you using? They vary a great deal in terms of the PLL.

 

0 Kudos
Reply

1,476 Views
admin
Specialist II

yeah hello peg,

thank you 4 d response..

I am using a Demokit of SK-S12XDP512A from HCS12X (Softech)

I am asked to measure the parameters of an input signal from a function generator..

but where do i actually see the output?

 

0 Kudos
Reply