PLL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PLL

1,981件の閲覧回数
admin
Specialist II

Hello,

can anyone please tell me in detail how the PLL is enabled ,what and how are the calculations for the clock done?

I want to write a program using interrupts to measure the frequency of an input signal where modules like PLL, ECT are to be used. What kind of interrupt would it be like? 

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,477件の閲覧回数
peg
Senior Contributor IV

Hello manasa,

 

As this is a hardware related question you should be posting in the appropriate hardware forum.

Also which device are you using? They vary a great deal in terms of the PLL.

 

0 件の賞賛
返信

1,477件の閲覧回数
admin
Specialist II

yeah hello peg,

thank you 4 d response..

I am using a Demokit of SK-S12XDP512A from HCS12X (Softech)

I am asked to measure the parameters of an input signal from a function generator..

but where do i actually see the output?

 

0 件の賞賛
返信