PKGPPCNEXUSSTARTER_install

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PKGPPCNEXUSSTARTER_install

Jump to solution
5,136 Views
smallyang
Contributor IV

smallyang_0-1711185323398.pngsmallyang_0-1711185323398.png

是这样的我安装了cw v2.10 ,它自带的PE Micro 看起来版本太低了老是显示无法进入后台

Here's the thing: I installed cw v2.10, and it comes with a PE Micro that looks too low and keeps showing that I can't get into the background

smallyang_1-1711185512817.pngsmallyang_1-1711185512817.png

 

然后我在论坛看到说1.34版本太低要给它升级一下,然后我就去升级了最新的8.98版本,然后它说我硬件太旧让我以旧换新,这显然是无法实现的,然后我又另外找了5.12和7.59的版本,它们都有一个相同的问题:我输入install code 没有生成蓝色的registration code ,请问有人知道怎么解决吗?

Then I saw in the forum that version 1.34 was too low to upgrade it, then I went to upgrade the latest version 8.98, then it said my hardware was too old and asked me to trade it in, which is obviously not possible, then I found another version 5.12 and 7.59, they both have the same problem: I input install code and no blue registration code is generated. Does anyone know how to solve it?

 

这是别人的界面

This is someone else's interface

smallyang_2-1711185852135.pngsmallyang_2-1711185852135.png

 

 

这是我的界面

This is my interface

smallyang_3-1711185852137.pngsmallyang_3-1711185852137.png

 

 

0 Kudos
Reply
1 Solution
5,009 Views
smallyang
Contributor IV

升级版本后已解决

View solution in original post

0 Kudos
Reply
3 Replies
5,010 Views
smallyang
Contributor IV

升级版本后已解决

0 Kudos
Reply
4,059 Views
xierxiaofeng
Contributor II
您好,
现在我遇到的情况和您的一样,请问您是怎么解决的?
谢谢!
0 Kudos
Reply
4,037 Views
smallyang
Contributor IV

You can update your CW2.10 by reading this FAQ and getting the "Patch for Qorivva (PowerPC Nexus) Codewarrior"
https://www.pemicro.com/faqs/faq_view.cfm?id=211&menu_id=faqs

 

 

这是PE官网的解答

https://www.pemicro.com/forums/forum_topic.cfm?forum_id=9&forum_topic_id=8816#c30821

 

 

0 Kudos
Reply