PEMicro TraceLink trace ends prematurely

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PEMicro TraceLink trace ends prematurely

2,249 Views
robertgrimshaw
Contributor I

I'm having a problem using my PEMicro Tracelink with CodeWarrior, attempting to trace the execution of firmware on a Cortex-M0+.  The trace ends prematurely, well before the 128Mb of configured trace buffer is filled.  Oddly, each trace seems to stop after a different number of trace records, sometimes in the 3k range, sometime in the 5k range.  When the trace stops, it halts the processor and drops me into the debugger at a return from a function, in code that I was expecting to be running.  

I have the "Trace Max Buffer Size" option set to 128 Mb in the target settings, and in the Trace and Profile settings I have the "Trace Buffer Size" set to 0x2000, with "Continuous" selected.  

I'm tracing third-party code, so I'm stuck without source, but I can set a breakpoint where I want to begin trace and that works well.  The problem is that the assembly should clearly be looping for a very long time but something is happening that exits the loop and I want to know what.  Interrupts are disabled, but I was hoping a trace would catch an interrupt if that was the culprit and I was simply misunderstanding the assembly.  

Thanks in advance for the assistance.

Tags (2)
0 Kudos
Reply
3 Replies

2,112 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Robert,

Is this problem of the trace ending prematurely just happening with this project? Which CodeWarrior version are you using? I think that the following posts created by our colleague Erich Styger might be helpful for you:

First Steps with the P&E Tracelink | MCU on Eclipse 

Debugging ARM Cortex-M0+ Hard Fault with MTB Trace | MCU on Eclipse 

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply

2,112 Views
robertgrimshaw
Contributor I

I never did get to the bottom of this, but the premature trace stops may have been occurring when the watchdog timer was resetting the chip.  Code I added was not servicing the timer and this was causing resets.  I got no indication of that in CodeWarrior, but that may have been what was happening.  

0 Kudos
Reply

2,112 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Robert,

 

I agree with you, the watchdog reset was most likely causing the trace to stop.

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply