PE - bug in I2C for DSC utility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PE - bug in I2C for DSC utility

ソリューションへジャンプ
1,671件の閲覧回数
Ben
Senior Contributor I

Hello

I tried to use the I2C_RecvBlock for DSC (8257) - it does not work good.

It should send address in write mode, and switch to read mode without sending a STOP bit.

It enter read mode and read the number of bytes I need, but without sending the address first.

I work with CW 11 and automatic STOP option ON.

Is there a new PE addon ?

1 解決策
1,547件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Yes, you can disable code generation in different ways, and you can do it for a single component too, see Disable my Code Generation | MCU on Eclipse 

I hope this helps,

Erich

元の投稿で解決策を見る

3 返答(返信)
1,547件の閲覧回数
Ben
Senior Contributor I

OK, I found the problem in PE code, and corrected it.

Q: Is there a way to freeze only the IIC file so PE will not run over the changes I made?

0 件の賞賛
返信
1,548件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Yes, you can disable code generation in different ways, and you can do it for a single component too, see Disable my Code Generation | MCU on Eclipse 

I hope this helps,

Erich

1,547件の閲覧回数
Ben
Senior Contributor I

Thanks Erich, it's a pity that I saw your response only today... I disabled this module auto-generation, and started to smile again :-)