Open Declaration issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Open Declaration issue

跳至解决方案
1,915 次查看
joseefrenrodrig
Contributor I

Hi, my name is J. Efren Rodriguez and I have an issue with Code Warrior 10.2. My software works ok but its no possible to navigate in it.


The code compiles, generate the binary files and also runs in the pcb board I designed but I can navigate in the code.


Let me explain....


The open declaration or F3 funtions doesnt do anything.


I open the c file, main in this case, select the port B define and press F3. Nothing happens. It is in all the funtions, defines or subroutines. When I download the code in my pcb board,it works right


Could anyone explain me the linker paths I must check to be able to navigate?


Thanks in advice.

 


标签 (1)
0 项奖励
回复
1 解答
1,641 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

this sounds like an issue with the Eclipse indexer. Have a look at

Fixing the Eclipse Index | MCU on Eclipse

This probably will help.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,642 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

this sounds like an issue with the Eclipse indexer. Have a look at

Fixing the Eclipse Index | MCU on Eclipse

This probably will help.

0 项奖励
回复