Open Declaration issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Open Declaration issue

ソリューションへジャンプ
1,920件の閲覧回数
joseefrenrodrig
Contributor I

Hi, my name is J. Efren Rodriguez and I have an issue with Code Warrior 10.2. My software works ok but its no possible to navigate in it.


The code compiles, generate the binary files and also runs in the pcb board I designed but I can navigate in the code.


Let me explain....


The open declaration or F3 funtions doesnt do anything.


I open the c file, main in this case, select the port B define and press F3. Nothing happens. It is in all the funtions, defines or subroutines. When I download the code in my pcb board,it works right


Could anyone explain me the linker paths I must check to be able to navigate?


Thanks in advice.

 


ラベル(1)
0 件の賞賛
返信
1 解決策
1,646件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

this sounds like an issue with the Eclipse indexer. Have a look at

Fixing the Eclipse Index | MCU on Eclipse

This probably will help.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,647件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

this sounds like an issue with the Eclipse indexer. Have a look at

Fixing the Eclipse Index | MCU on Eclipse

This probably will help.

0 件の賞賛
返信