On chip flash programming in MC68HC908QB8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

On chip flash programming in MC68HC908QB8

ソリューションへジャンプ
4,058件の閲覧回数
kuji83
Contributor I
Hi,
In MC68HC908QB8, How can we access the falsh area and do page erase, Programming and Check or Compare programing. Any conversant c code available to all functions.
 
We would like to erase the falsh area and update with datas and do comparision with them and store these values.
 
Awaiting for reply.
 
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,617件の閲覧回数
J2MEJediMaster
Specialist I
Go the FAQ system and search for "Flash programming". A number of FAQs on the subject should show up. You'll have to sift through these for your MCU. Some of them reference Application notes, which document how to use a feature, such as programming Flash, and even provide source code.

---Tom

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,617件の閲覧回数
kuji83
Contributor I
Thank you very much for your help.I have wriiten the flash routine.
0 件の賞賛
返信
2,617件の閲覧回数
bigmac
Specialist III
Hello,
 
The application notes AN2635 and AN2874 cover use of the ROM-resident routines, present within the QB8, and other HC908 devices.
 
Regards,
Mac
 
2,617件の閲覧回数
CrasyCat
Specialist III
Hello
 
Did you check application notes on Freescale web site?
 
There might be something in there.
 
CrasyCat
0 件の賞賛
返信
2,618件の閲覧回数
J2MEJediMaster
Specialist I
Go the FAQ system and search for "Flash programming". A number of FAQs on the subject should show up. You'll have to sift through these for your MCU. Some of them reference Application notes, which document how to use a feature, such as programming Flash, and even provide source code.

---Tom
0 件の賞賛
返信