Not breaking on breakpoint

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not breaking on breakpoint

ソリューションへジャンプ
2,898件の閲覧回数
zwilcox
Contributor IV

I'm using a PE Micro USB Multilink Interface module to connect to my target.  Also using CodeWarrior 11.0.0 on Windows 10.

 

I have been having troubles breaking at breakpoints, so I placed a break point in a loop.

 

When I invoke the debugger, the source comes up in the left window/panel and the debugger is sitting at right after main.   As you can see, I have three break point set at Line 22, 23, and 24.  The breakpoints are a Regular, Hardware, and Software.

So, at this point, I click on the "Resume" icon (green triangle just under "Run" in top menu).  Execution does not stop at the break point. 

Any ideas on why I can't break at breakpoints that I set?

タグ(2)
1 解決策
2,766件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Zachary Wilcox,

It seems you have disable all the breakpoints, please click the below button to enable it :

pastedImage_1.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,767件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Zachary Wilcox,

It seems you have disable all the breakpoints, please click the below button to enable it :

pastedImage_1.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------