No Vpp Programming Voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No Vpp Programming Voltage

Jump to solution
3,922 Views
Philou
Contributor I
Hi guys
 
i'm trying to debug a S12X software, and i have this issue, no programming voltage. i have suspected a board issue. but on another one it's the same issue.
i have that on the command display:
Vppon command file correctly executed.
FP: No programming voltage
FP: No programming voltage
FP: ALL_PPAGES flash module is bad or protected.
executing .\cmd\P&E_Multilink_CyclonePro_vppoff.cmd
 
i have tried to unsecure the chip, but when i do that the debbugger crashes.
 
Any thoughts?
 
Thanks for your help.
 
Philou
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,632 Views
Philou
Contributor I
Found the issue. Even if I have checked that on the rising edge of the reset the state of MODA and MODB (low), it was not sufficient. Theses pins must be pulled down no for setting the correct MCU mode.

View solution in original post

0 Kudos
Reply
1 Reply
1,633 Views
Philou
Contributor I
Found the issue. Even if I have checked that on the rising edge of the reset the state of MODA and MODB (low), it was not sufficient. Theses pins must be pulled down no for setting the correct MCU mode.
0 Kudos
Reply