No Vpp Programming Voltage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No Vpp Programming Voltage

ソリューションへジャンプ
3,927件の閲覧回数
Philou
Contributor I
Hi guys
 
i'm trying to debug a S12X software, and i have this issue, no programming voltage. i have suspected a board issue. but on another one it's the same issue.
i have that on the command display:
Vppon command file correctly executed.
FP: No programming voltage
FP: No programming voltage
FP: ALL_PPAGES flash module is bad or protected.
executing .\cmd\P&E_Multilink_CyclonePro_vppoff.cmd
 
i have tried to unsecure the chip, but when i do that the debbugger crashes.
 
Any thoughts?
 
Thanks for your help.
 
Philou
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,637件の閲覧回数
Philou
Contributor I
Found the issue. Even if I have checked that on the rising edge of the reset the state of MODA and MODB (low), it was not sufficient. Theses pins must be pulled down no for setting the correct MCU mode.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,638件の閲覧回数
Philou
Contributor I
Found the issue. Even if I have checked that on the rising edge of the reset the state of MODA and MODB (low), it was not sufficient. Theses pins must be pulled down no for setting the correct MCU mode.
0 件の賞賛
返信