Need code for SCI communication with interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need code for SCI communication with interrupt

ソリューションへジャンプ
2,557件の閲覧回数
Ryu
Contributor I
Hello.
I have an EVB9S12NE64 board and I simply need to setup it up to read-in data through SCI1 using interrupt. Is there a good self explained code example I could use with my little knowledge in the field of embedded devices?

Thanks in advance.
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,612件の閲覧回数
CrasyCat
Specialist III
Hello
 
I would recommend you to try to create a project with ProcessorExpert support.
You can then configure what you want to do with your SCI interrupt and let Processor Expert generate code for you.
 
Processor Expert will generate working application. You can then choose whether you want to continue to work with ProcessorExpert or if you want to take the generated code as a template that you integrate in your own application.
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,613件の閲覧回数
CrasyCat
Specialist III
Hello
 
I would recommend you to try to create a project with ProcessorExpert support.
You can then configure what you want to do with your SCI interrupt and let Processor Expert generate code for you.
 
Processor Expert will generate working application. You can then choose whether you want to continue to work with ProcessorExpert or if you want to take the generated code as a template that you integrate in your own application.
 
CrasyCat
0 件の賞賛
返信