Need code for SCI communication with interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need code for SCI communication with interrupt

Jump to solution
2,546 Views
Ryu
Contributor I
Hello.
I have an EVB9S12NE64 board and I simply need to setup it up to read-in data through SCI1 using interrupt. Is there a good self explained code example I could use with my little knowledge in the field of embedded devices?

Thanks in advance.
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,601 Views
CrasyCat
Specialist III
Hello
 
I would recommend you to try to create a project with ProcessorExpert support.
You can then configure what you want to do with your SCI interrupt and let Processor Expert generate code for you.
 
Processor Expert will generate working application. You can then choose whether you want to continue to work with ProcessorExpert or if you want to take the generated code as a template that you integrate in your own application.
 
CrasyCat

View solution in original post

0 Kudos
Reply
1 Reply
1,602 Views
CrasyCat
Specialist III
Hello
 
I would recommend you to try to create a project with ProcessorExpert support.
You can then configure what you want to do with your SCI interrupt and let Processor Expert generate code for you.
 
Processor Expert will generate working application. You can then choose whether you want to continue to work with ProcessorExpert or if you want to take the generated code as a template that you integrate in your own application.
 
CrasyCat
0 Kudos
Reply