Missing file MBit1.hI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Missing file MBit1.hI

1,268 次查看
juliancox
Contributor V

I cannot implement BItIO or BItsIO. I used Processor Expert to configure my on-chip components, but when I build the project it fails  with the message: -

mingw32-make: *** No rule to make target `XXX/Generated_Code/MBit1.h', needed by `Sources/Events_c.obj'.  Stop.

(file name and path left out for copyright purposes)

I find that file MBit1.h does not exist on my computer. Other components (ByteIO, FreeCntr) work fine

work fine.

I am using Version 10.7

3 回复数

1,088 次查看
juliancox
Contributor V

Hi Carlos,

I am using a MC9S08QE128on a DEMOQE board. However, since posting this question a very strange thing happened. I decided that, while waiting for a solution to my problem,  I would carry on writing my application code. Using Processor Expert, I added a counter (FC1) and both BitIO and BitsIO and it compiled without error, BUT having checked everything there is no #include "MBit1.h" anywhere in the project, especially Events.c.

1,088 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Julian,

 

It is good to hear the problem has been fixed, please let us know if the issue come up again.

 

Best Regards!
Carlos Mendoza
Technical Support Engineer

0 项奖励
回复

1,088 次查看
Carlos_Mendoza
NXP Employee
NXP Employee


Hi Julian,

Could you tell us which MCU are you using?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 项奖励
回复