Misaligned long word access interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Misaligned long word access interrupt

1,918 Views
pgillaspy
Contributor III

I am using CW 11.1 with DSC 2.7.3 on MC56F83000-EVK.  When I call a subroutine from an ISR I get vectored to the following default  interrupt routine:

/* misaligned long word access interrupt ($0A) */

#ifndef INT_VECTOR_ADDR_5
#define INT_VECTOR_ADDR_5 misalign

static asm void misalign(void)
{
debughlt
nop
rti
}

#endif

If I do not call the subroutine, the ISR performs correctly.  What is the cause of this misaligned long word access interrupt error?

0 Kudos
Reply
2 Replies

1,898 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you post the ISR code which will fire the unaligned ISR?

As a workaround, if the api function you called in ISR takes a long time, I suggest you just set a bool flag in the ISR, in the main while(1), you can poll the flag, if it is set, call the api function, then clear the flag.

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply

1,894 Views
pgillaspy
Contributor III

Having continued to develop the code for other functionality, the misaligned long word acccess has gone away.  If it pops up again, I will post the offending code.

0 Kudos
Reply