Memory Usage for MC9S08QB8 Device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Memory Usage for MC9S08QB8 Device

Jump to solution
2,444 Views
bpaehr
Contributor IV

When I access the CodeWarrior Debugger, a Console Window named "<project>_Flash_PnE U-Multilink" opens which shows a bunch of "INF" lines.  The following lines are part of that output:

 

INF: CMD>VC

 

INF: Verifying object file Checksum16+CRC8 to device ranges ...

 

INF:    block 0000E000-0000E735 ...

 

INF: Ok.

 

INF:    block 0000FFE6-0000FFE7 ...

 

INF: Ok.

 

INF:    block 0000FFFE-0000FFFF ...

 

INF: Ok.

 

INF:    Checksum Verification Successful. (Cumulative Checksum16+CRC8=$E1FEAC)

 

Do I assume that the E000-E735 is absolutely ALL of the Flash memory that my code occupies, and only two vectors for RESET and the TIMER that I defined for use are being written to the Flash memory?  And that this is a quick way to determine how much Flash memory my code occupies?

 

In regards to the amount of RAM used, I found the following in the MAP file:

 

MODULE STATISTIC

  Name                                      Data   Code  Const

---------------------------------------------------------------------------------------------

  Utilities_c.obj                              44    472      0

  main_c.obj                                  21    524      2

  start08_c.obj                                0    132      0

  mc9s08qb8_c.obj                       72      0       0

  rtshc08.o (ansiis.lib)                     0    697      0

  other                                           64     16       7

 

The "Code" column totals add up to 0x0731, which seems to coincide with the reported E000-E735 range.  Do I then assume that the Data column shows ALL of the RAM memory used by the project, for a total of 201 bytes?  And how do the "Const" bytes (which I assume represent Constants) figure into memory usage?

 

I am using CW10.6.4 for an MC9S08QB8 device.

Thank you, in advance.

Labels (1)
1 Solution
2,245 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi BOB,

yes. correct. "Summary of section sizes per section type:" section is the right place to check the memory usage.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,245 Views
bpaehr
Contributor IV

Looking further, I also found the following in the MAP file:

Summary of section sizes per section type:

READ_ONLY (R):         73A (dec:     1850)

READ_WRITE (R/W):     81 (dec:      129)

NO_INIT (N/I):                 48 (dec:       72)

The "73A" is close to the Flash value range, and the 129 + 72 adds up to the same 201 value, so this section of the MAP file can be used as a double-check of the Flash and RAM usage?

0 Kudos
Reply
2,246 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi BOB,

yes. correct. "Summary of section sizes per section type:" section is the right place to check the memory usage.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------