When I access the CodeWarrior Debugger, a Console Window named "<project>_Flash_PnE U-Multilink" opens which shows a bunch of "INF" lines. The following lines are part of that output:
INF: CMD>VC
INF: Verifying object file Checksum16+CRC8 to device ranges ...
INF: block 0000E000-0000E735 ...
INF: Ok.
INF: block 0000FFE6-0000FFE7 ...
INF: Ok.
INF: block 0000FFFE-0000FFFF ...
INF: Ok.
INF: Checksum Verification Successful. (Cumulative Checksum16+CRC8=$E1FEAC)
Do I assume that the E000-E735 is absolutely ALL of the Flash memory that my code occupies, and only two vectors for RESET and the TIMER that I defined for use are being written to the Flash memory? And that this is a quick way to determine how much Flash memory my code occupies?
In regards to the amount of RAM used, I found the following in the MAP file:
MODULE STATISTIC
Name Data Code Const
---------------------------------------------------------------------------------------------
Utilities_c.obj 44 472 0
main_c.obj 21 524 2
start08_c.obj 0 132 0
mc9s08qb8_c.obj 72 0 0
rtshc08.o (ansiis.lib) 0 697 0
other 64 16 7
The "Code" column totals add up to 0x0731, which seems to coincide with the reported E000-E735 range. Do I then assume that the Data column shows ALL of the RAM memory used by the project, for a total of 201 bytes? And how do the "Const" bytes (which I assume represent Constants) figure into memory usage?
I am using CW10.6.4 for an MC9S08QB8 device.
Thank you, in advance.