Marco error of CW10.6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Marco error of CW10.6

1,643 次查看
kehanqin-b46569
NXP Employee
NXP Employee

Hi,experts

I am helping customer to create a calendar , the code I once used on K60, now I migrate it to PT60,platform is not problem but point is as long as I used marco to define count and use in algorithm, the value go crazy...

It maybe some setting of CW10.6  cause it.

Please see the picture below:

use the lower part, work fine, use upper, once the time go around 3 hours 40 minutes, the year will add 1 directly.

17844_17844.pngcalendar issue.png

and a other problem, I cannot multiply "one" element of a structure directly, once used, value go crazy again...

I must give it to a variable first, then works fine.

even so, still cannot use marco instead of 3600, will reach a wrong value.

17845_17845.pngcalendar issue 1.png

17849_17849.pngcalendar issue_1.png

 

My code attached, thanks!

Original Attachment has been moved to: GREE-COOKER-TEST-TSI-MTIM-Calendar.zip

标签 (1)
标记 (2)
0 项奖励
回复
2 回复数

1,448 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Kehan,

const define is recognized as int by default. if we want to use it as other type in computation, we need to cast it with exact variable type.

Best Regards,

Zhang Jun

=============================================

this answer is for you, if it helps, please click on "Correct Answer" button, thanks!

0 项奖励
回复

1,448 次查看
CompilerGuru
NXP Employee
NXP Employee

Is the issue that sizeof(int) is 2 in your target?

If so, then SEC_OF_DAY overflows in the macro computation.

To make the computation as unsigned long, add a ul suffix to one of the numbers.

E.g.

#define SEC_OF_DAY ( SEC_OF_HOUR * 24uL)

0 项奖励
回复