MRAM debug (programming) does not work on MQX4.0????

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MRAM debug (programming) does not work on MQX4.0????

跳至解决方案
1,813 次查看
CarlFST60L
Senior Contributor II

Hi,

 

I am running CW4.0, MQX4.0 and the hello world MRAM debug and it will not program MRAM (boot exception). Debug and Release work fine. This is a problem I had in CW10.3 which was noted by the developers and said to be fixed in CW10.4. I finally got to test this feature this morning and it doesn't work in our project, or, in the example project.

 

Attached is the debug log of the programmer (I am using cyclone max ethernet and USB, the log is from my ethernet attempt)

 

I really need this to work as CW10.2 is a complete pile of rubbish with a million bugs and work arounds, we waste a few hours a week on 10.2 and its various issues. I have been using CW10.4 all week on a project with no MRAM and its amazing!

Original Attachment has been moved to: MRAM_HELLO_WORD_DEBUG_TRACE.txt.zip

标签 (1)
0 项奖励
回复
1 解答
1,621 次查看
CarlFST60L
Senior Contributor II

Ok, so, computer restart fixed it... wow....

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,622 次查看
CarlFST60L
Senior Contributor II

Ok, so, computer restart fixed it... wow....

0 项奖励
回复