MPC5644A GPIO-GPDO Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5644A GPIO-GPDO Error

1,403 Views
tgc-yilmaz
Contributor III

Hello,
I'm using mpc5644a. I have set the 124th pin as GPIO output pin. However, I have observed that the value assigned to register GPDO [124] is set in register GPDO [123]. At the same time, I observed that this happened from pin 101 to pin 145. (Address has been defined twice for GPDO [101].) 

tgc-yilmaz_0-1599058462962.png

NOTE: The same is true for GPDI[101]. However, no shift was observed in the GPDI[] registers.

What is the reason for this situation?

If there is an error, is there a published error record that describes this situation? Can you help with this?

Thanks in advance.

0 Kudos
Reply
0 Replies