MK70 UART Module clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK70 UART Module clock

1,324 Views
codybennett
Contributor I

I am in the process of setting up the UART Baud on an MK70FN1M0VMJ12 (custom board). I need to know how to verify/set the Module Clock frequency. It seems this is derived from the Bus clock yet I have not found a register to set or verify for the frequency.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,200 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

pastedImage_0.png

so , you should be sure the number of UART.

Then we can refer to the clocking didagram calculate the system clock or  bus clock , please see :

pastedImage_1.png

And each part can be found the related register on the RM.

Hope it helps

Alice

0 Kudos
Reply