MISRA-C checker for CodeWarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MISRA-C checker for CodeWarrior

5,041 Views
peterkrause
Contributor I

Hello.

 

I'm using CodeWarrior 10.6 with a Kinetis K10. I'm looking for a code checker for MISRA-C 2004.

Is there any option to get a plugin/add-on to enable MISRA checking in CodeWarrior?

 

Regards

Peter Krause

Labels (1)
Tags (3)
0 Kudos
Reply
4 Replies

3,520 Views
BlackNight
NXP Employee
NXP Employee

Hi Peter,

one option is to use PC-lint, for which there is a plugin (unfortunately not free):

http://mcuoneclipse.com/2012/04/01/eclipse-and-pc-lint-linticator/

There is another way without a plugin:

Linting without a plugin | MCU on Eclipse

Regards,

Erich

0 Kudos
Reply

3,520 Views
peterkrause
Contributor I

Hi Erich.

thanks for your reply. The combination of Linticator and PC-Lint looks great. But there is no trial version for PC-Lint and I would like to test it before buying.

Regards

Peter

0 Kudos
Reply

3,520 Views
trytohelp
NXP Employee
NXP Employee

Hi Peter,

I don't know their business model but you can contact Gimpel:

      http://www.gimpel.com/html/index.htm


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,520 Views
peterkrause
Contributor I

Hi Pascal,

I contacted Gimpel already and asked for a trial version. But they don't offer a trial version. You can only test some code in your browser to test PC-Lint.

Regards

Peter Krause

0 Kudos
Reply