MCF5329 bring-up issue with CW V7.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5329 bring-up issue with CW V7.2

ソリューションへジャンプ
1,271件の閲覧回数
smanni
Contributor II

Hi,

 

I'm facing an issue while trying to bring-up an MCF5329 using CodeWarrior V7.2 and a P&E multilink USB.

 

Here is what I did:

 

  1. create a bareboard project using the wizard
  2. generate initialization code with Process Expert
  3. use the default initialization script (.cfg) and memory description script (.mem) [attached]
  4. use the default linker script [attached]
  5. compile
  6. debug

 

Here I get an error on memory verify after write:

Failed writing target address 0x80000500.
Expected value: 0x80007ffc
Actual value: 0x0

 

If I disable the "verify after write" option from debug menu it can go farther but never reach _startup() and in addition memory is all set to zero (except for reserved areas where I see 0xBA) and registers are all zero.

 

NOTE: If I use CodeWarrior V10.6.4 and proceed the same (basic project by wizard, etc.) I have no problems.

 

Do you have any idea how to solve this issue? In CW10 the debug configuration has more options than CW7 but practically they seems to me to be equal. Would you advise me on some of these?

 

Thanks.

Regards,

Stefano

Original Attachment has been moved to: MCF5329_INTERNAL_RAM.mem.zip

Original Attachment has been moved to: MCF5329_INTERNAL_RAM.lcf.zip

Original Attachment has been moved to: MCF5329_INTERNAL_RAM.cfg.zip

ラベル(1)
0 件の賞賛
返信
1 解決策
1,068件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Please submit this issue to correct community, it should be CodeWarrior for MCU

元の投稿で解決策を見る

1 返信
1,069件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Please submit this issue to correct community, it should be CodeWarrior for MCU