MCF51QE128 How to place program code into RAM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF51QE128 How to place program code into RAM?

Jump to solution
2,851 Views
Andik
Contributor II

Hello,


I would like to write small application, which should run from RAM (MCF51QE128). Code will be downloaded to RAM after power up, so I don't want do any copy from FLASH. Can anybody help me with CW HC08 6.1? How could this be done? I'm turning from HCS08 assembly to CFV1 C language so I found this a bit complicated.


Another view on this problem, if I could force compiler to use relative addressing for jumps, conditions, data, the code could be moved anywhere in memory space, also into RAM, how to achieve (configure) this?


Many thanks for helpful ideas...

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,931 Views
CrasyCat
Specialist III

Hello

 

Can you take a look at FAQ-27860 on www.freescale.com.

 

This should provide you the information you need

 

CrasyCat

View solution in original post

0 Kudos
Reply
2 Replies
1,932 Views
CrasyCat
Specialist III

Hello

 

Can you take a look at FAQ-27860 on www.freescale.com.

 

This should provide you the information you need

 

CrasyCat

0 Kudos
Reply
1,931 Views
Andik
Contributor II

CrasyCat,
thank you for useful info.

0 Kudos
Reply