MC56F8357 - external RAM Test

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC56F8357 - external RAM Test

ソリューションへジャンプ
1,924件の閲覧回数
vineethcn
Contributor I

Hello All,

 

     I'm working on external data RAM with the DSC MC56F8357. I am able to read and write external RAM.  I use CW 8.3 version and In linker command file (.cmd) i defined external memory address range and added section definition. In code i use Pragma, this every thing works fine for me. But now i need to add a test code to test the external RAM.

Kindly guide me how to develop the external RAM test code. All your comments and guidelines/notes are most welcome.

 

Thanks.

Vineeth

ラベル(1)
0 件の賞賛
返信
1 解決策
1,663件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Vineeth

There is no difference to test the external RAM with internal RAM or any other memory type (e.g. internal flash). 

The common method is verification by writing and reading back. Or you may use CRC check.  On this point, external memory is not special. 

Best Regards

Fiona Kuang

Technical Information & Commercial Support

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,664件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Vineeth

There is no difference to test the external RAM with internal RAM or any other memory type (e.g. internal flash). 

The common method is verification by writing and reading back. Or you may use CRC check.  On this point, external memory is not special. 

Best Regards

Fiona Kuang

Technical Information & Commercial Support

0 件の賞賛
返信