Looking for the memory map header file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Looking for the memory map header file

ソリューションへジャンプ
3,490件の閲覧回数
nocturnalHippoz
Contributor I

Hi everyone,

 

I'm looking for memory map header file where I can change the RAMStart and RAMend addresses.

I'm currently using CodeWarrior for  writing to the 9S12C32 (via Technological Art's Esduino board rev. 1).

The start and end should be: $3800 to $3FFF. However, everytime I begin a new project, the default values are

$0800 to $0FFF.

 

When I start a new project in assembly, I can access the "mc9s12c32.inc" and change the RAMStart and RAMEnd.

However, in a new project in C, I can seem to find a similar header file to change it.

 

Thank you in advance.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,946件の閲覧回数
Lundin
Senior Contributor IV

To map the RAM differently you need to do the following:

 

In the PRM file change the addresses. For example, this maps RAM from 0x2000 to 0x3FFF, with reserved space for the stack.

 

SEGMENTS
    STACK_RAM     = READ_WRITE   0x2000  TO    0x24FF;
    RAM      = READ_WRITE   0x2500  TO    0x3FFF; 
END
 
PLACEMENT
    .stack                       INTO  STACK_RAM;
END
 
STACKSIZE 0x500
 

Note: the stack should be placed below the rest of the RAM in the memory map. That way, a stack overflow will write to illegal addresses yielding an error, instead of silently trashing your whole RAM.

 

Whether you write in assembler or C, you will then have to write to the RAM mapping register INITRM (the CW debugger can handle such memory mapping writes in runtime). This is best done directly from the reset vector. Example:

 

void interrupt_reset(void)
  {
    #pragma MESSAGE DISABLE C12053
    asm LDS   #$2500;                   /* set stack */
   
    INITRM   = 0x21;                        /* map RAM */
  
    asm CALL main;
  }

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,947件の閲覧回数
Lundin
Senior Contributor IV

To map the RAM differently you need to do the following:

 

In the PRM file change the addresses. For example, this maps RAM from 0x2000 to 0x3FFF, with reserved space for the stack.

 

SEGMENTS
    STACK_RAM     = READ_WRITE   0x2000  TO    0x24FF;
    RAM      = READ_WRITE   0x2500  TO    0x3FFF; 
END
 
PLACEMENT
    .stack                       INTO  STACK_RAM;
END
 
STACKSIZE 0x500
 

Note: the stack should be placed below the rest of the RAM in the memory map. That way, a stack overflow will write to illegal addresses yielding an error, instead of silently trashing your whole RAM.

 

Whether you write in assembler or C, you will then have to write to the RAM mapping register INITRM (the CW debugger can handle such memory mapping writes in runtime). This is best done directly from the reset vector. Example:

 

void interrupt_reset(void)
  {
    #pragma MESSAGE DISABLE C12053
    asm LDS   #$2500;                   /* set stack */
   
    INITRM   = 0x21;                        /* map RAM */
  
    asm CALL main;
  }

 

0 件の賞賛
返信
2,946件の閲覧回数
nocturnalHippoz
Contributor I

Thank you Lundin :smileyhappy:

0 件の賞賛
返信